Add an HMI Device
To control an application,
It can also be embedded into targeted Controllers.
- Modbus TCP is used for communication from an HMI panel's Ethernet port to the X32 connector on the top of a AKD PDMM or PCMM.
- Modbus communication may be active while programming the controller through the KAS-IDE while the AKD PDMM or PCMM is connected to a network, switch, or hub.
- The KAS-IDE is automatically linked to the KVB HMI development software, and the Modbus addresses are automatically set.
- See KDN for more information.
When running the KAS Simulator, an internal HMI editor is also available to debug the application.